LPCxpresso546

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCxpresso546

4,540 次查看
blair_smyth
Contributor I

Hi There,

I am using the LPCXpresso546 EVM and i believe i have a build on the EVM that has hard faulted and cannot seem to conect the device to my IDE.

The probe cannot be found and i am using CMSIS DAP.

Is there a way i can erase what is on the device and reconnect?

Kind regards,

Blair

0 项奖励
回复
10 回复数

4,519 次查看
frank_m
Senior Contributor III

> The probe cannot be found and i am using CMSIS DAP.

This sounds like you somehow damaged it physically. The debug adapter and target are mostly independant, so the CMSIS-DAP should be found when the proper PC driver is installed.

However, they are "linked" via the power supply. If the EVM has such a possibility, check the current consumption. And/or check the supply voltages (+5V, +3.3V).

0 项奖励
回复

4,503 次查看
blair_smyth
Contributor I

Hi there,

 

Thanks for the reply, ive recently gotten myself a new EVM straight out of the box, i cannot seem to see the device on my computer through device manager and my IDE still cannot find the probe.

Any other ideas where i might be going wrong?

Thanks,

Blair

0 项奖励
回复

4,497 次查看
converse
Senior Contributor V

If you haven't already try different USB ports on your computer. Also try changing the USB cable. Finally, make sure you are connecting to the correct port on the large board.

0 项奖励
回复

4,493 次查看
frank_m
Senior Contributor III

Or a different PC. It should at least show up as unknown USB device, check the device manager (under Windows).

0 项奖励
回复

4,487 次查看
blair_smyth
Contributor I

I have tried different USB ports, tried my other laptop and still isnt recognised.

I have the USB connected to j8 and perform a software reset, holding down ISP0 and toggling reset, but still no connection showing in the device manager, even as an unknown device.

I am able to use a UART programming tool and have loaded the gpio_led_output program from the SDK to the device and when loaded pressing SW2 does illuminate LED3.

So it seems the EVM is working correctly but i just cannot connect to it over USB to program or to debug with my IDE.

Blair

0 项奖励
回复

4,478 次查看
converse
Senior Contributor V

You may need to use JP5 and LPCScrypt to reload the debug firmware image.

0 项奖励
回复

4,464 次查看
blair_smyth
Contributor I

Do you or anyone have the correct link for the LPCScrypt?

The one i am trying to run doesnt seem to work.

I am trying to run LPCScrypt v2.1.2 Nov 2020

0 项奖励
回复

4,457 次查看
converse
Senior Contributor V

That is the latest version of LPCScrypt.

Please explain what you mean by "doesn't seem to work" - describe what happens, any messages etc.

0 项奖励
回复

4,531 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Blair,

You said that you use LPCXpresso546 EVM, can you tell me the concrete board name in detail? for example the LPCXpresso54608 EVM or LPCXpresso54628 EVM.

Secondly, you said that you can not connect to the board, I think this is a trick, you can hold ISP0 button, then press/release Reset button, then you can try to download the code and check if you can communicate.

Regarding the hardfault, I suppose your code has issue, pls download an example code in SDK package and have a try.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复

4,525 次查看
blair_smyth
Contributor I

Hi Xiangjun,

I am using the LPCXpresso54628 EVM, I have tried to hold down the ISP0 button and reset, then i try to connect to the device but still no probe is found.

Even in my computers device manager there is no USB device detected.

I am able to connect to the device over UART and program bin files that way, and have uploaded an example project to the device, but i still cannot get a connection on j8 for USB.

Thanks,

Blair

0 项奖励
回复