LPCXpresso845MAX use ADC_Seqa_Seqb example code have pulse on ADC2 pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso845MAX use ADC_Seqa_Seqb example code have pulse on ADC2 pin

957 次查看
ristchen
Contributor II

Why LPCXpresso845MAX use ADC_Seqa_Seqb example code have pulse on ADC2(PIO14) pin when get ADC value?Inkedadc_LI.jpgTera_ADC.jpg

0 项奖励
回复
1 回复

947 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Chen,

I have checked the voltage spike on the PIO14/ADC2, I suppose this is a noise, the noise generally happens for the float input pins or high impedance input pin.

I suggest that you can connect a RC circuit for the ADC analog input channel. for example, this is a RC circuit, using 100 ohm and 2.2nF capacitor.

 

xiangjun_rong_0-1602566803097.png

Does the noise take effect on the ADC sample?

BR

XiangJun Rong

0 项奖励
回复