LPCXpresso845MAX use ADC_Seqa_Seqb example code have pulse on ADC2 pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso845MAX use ADC_Seqa_Seqb example code have pulse on ADC2 pin

951 Views
ristchen
Contributor II

Why LPCXpresso845MAX use ADC_Seqa_Seqb example code have pulse on ADC2(PIO14) pin when get ADC value?Inkedadc_LI.jpgTera_ADC.jpg

0 Kudos
Reply
1 Reply

941 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Chen,

I have checked the voltage spike on the PIO14/ADC2, I suppose this is a noise, the noise generally happens for the float input pins or high impedance input pin.

I suggest that you can connect a RC circuit for the ADC analog input channel. for example, this is a RC circuit, using 100 ohm and 2.2nF capacitor.

 

xiangjun_rong_0-1602566803097.png

Does the noise take effect on the ADC sample?

BR

XiangJun Rong

0 Kudos
Reply