LPCXpresso802 Power saving mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso802 Power saving mode

3,058件の閲覧回数
Babycat
Contributor III

Hello everyone,

May I check with you guy if there is anyone tested power saving mode with LPCXpresso802 kit?
I ran project "lpcxpresso802_power_mode_switch_lpc" and I got 4 options:

1. Sleep mode
2. Deep Sleep mode
3. Power Down mode
4. Deep power down mode

It surprised me that mode 4 (Deep power down mode) the consumption current is about 1mA which I think it is too much. I have measured on JP1 pins (3V3 source)
Any one please help to confirm?
I intend to use LPC802 for remote control, but 1mA is too much

Regards.

0 件の賞賛
返信
3 返答(返信)

3,026件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Babycat

In addition, please make sure you DISCONNECT the board with IDE debugger when measure. 

In default demo code, you need to select option 4 on hyper terminal to enter Deep power down mode. Try to revise the code to let LPC804 automatically go into deep lower down without remote control at the beginning code the main code.

download, power off and power on, Let the board run in standalone mode ( disconnect PC debugger)

Measure current again. You should be able to see consumption current down.

 

Have a nice day,

Jun Zhang

0 件の賞賛
返信

3,051件の閲覧回数
frank_m
Senior Contributor III

According to the user manual, JP7 is in the line between the user LEDs and VDD.

You would want JP1, which seems to be for such measurements.

However, I would check the schematics what current you measure in this case. Supply current for other, non-relevant parts might affect your measurement. I can't source the schematics on the fly ...

0 件の賞賛
返信

3,042件の閲覧回数
Babycat
Contributor III

  Hi Meyer

I have attached the schematic hereby, 

My VOM is between 2 pins of JP1, so only MCU current should flow through it.

Please have a check the attached schematic

Regards, 

0 件の賞賛
返信