LPCXpresso54628 Development Board SDRAM addressing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPCXpresso54628 Development Board SDRAM addressing

跳至解决方案
910 次查看
samv
Contributor II

I am using the documentation for the LPCXpress54628 development board as a guide to replicate the interface with the SDRAM IC IS42S16800F-6BLI in my own design.  I noticed on the diagram that there is a P1_24-EMC_A12 identified connected to pin G1.  However, the datasheet for that device shows pin G1 as NC.  I will assume it really isn't a functioning connection.  The 12 address lines A0-A11 do provide the 4K of addressing for the memory.  Was there a part change?  The other part number (W9812G6JB) also shows NC on G1.

Thanks

Sam

标签 (1)
0 项奖励
回复
1 解答
894 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @samv 

Yes, The W9812G6JB and IS42S16800F-6BLI both have only 12 bit address lines.

They are 128Mb SDRAM.

You can also check the LPC54628 RM.

Harry_Zhang_0-1739270013304.png

 

BR

Harry

在原帖中查看解决方案

0 项奖励
回复
1 回复
895 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @samv 

Yes, The W9812G6JB and IS42S16800F-6BLI both have only 12 bit address lines.

They are 128Mb SDRAM.

You can also check the LPC54628 RM.

Harry_Zhang_0-1739270013304.png

 

BR

Harry

0 项奖励
回复