LPCXpresso54628 Development Board SDRAM addressing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso54628 Development Board SDRAM addressing

Jump to solution
2,096 Views
samv
Contributor II

I am using the documentation for the LPCXpress54628 development board as a guide to replicate the interface with the SDRAM IC IS42S16800F-6BLI in my own design.  I noticed on the diagram that there is a P1_24-EMC_A12 identified connected to pin G1.  However, the datasheet for that device shows pin G1 as NC.  I will assume it really isn't a functioning connection.  The 12 address lines A0-A11 do provide the 4K of addressing for the memory.  Was there a part change?  The other part number (W9812G6JB) also shows NC on G1.

Thanks

Sam

Labels (1)
0 Kudos
Reply
1 Solution
2,080 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @samv 

Yes, The W9812G6JB and IS42S16800F-6BLI both have only 12 bit address lines.

They are 128Mb SDRAM.

You can also check the LPC54628 RM.

Harry_Zhang_0-1739270013304.png

 

BR

Harry

View solution in original post

0 Kudos
Reply
1 Reply
2,080 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @samv 

Yes, The W9812G6JB and IS42S16800F-6BLI both have only 12 bit address lines.

They are 128Mb SDRAM.

You can also check the LPC54628 RM.

Harry_Zhang_0-1739270013304.png

 

BR

Harry

0 Kudos
Reply