LPCXpresso54608 / OM13092 ISP mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso54608 / OM13092 ISP mode

3,334 Views
mirceaudrea
Contributor I

Hello,

I have a LPCXpresso54608 / OM13092 board and most probably I wrote the CRP incorrectly.

I get: Failed on connect: Ep(01). Target marked as not debuggable.

I need to erase the flash and regain debugger control. 

I tried to use Flash Magic with onboard LPC-LINK2(reset button +ISP0/1/2) on the serial port provided by it, but it cannot connect (cannot autobaud error).

Does the serial port on J13 connector provide ISP capabilities?

Is there another way in order to un-brick it?

Best regards,

Mircea

Labels (1)
0 Kudos
Reply
2 Replies

3,059 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Mircea Udrea,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.
Please refer to the attachment to assure the MCU enter the ISP mode successful via properly hardware configuration.
And I'd like to suggest another way to 'release' the LPC54608.
First, you should update the on-board LPC-Link2 with the JLink firmware,
then follow the Fig1 to work it out.
2017-04-27_10-27-44.jpgFig 1


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,059 Views
mirceaudrea
Contributor I

Did the job!

Thanks.

0 Kudos
Reply