LPCXpresso54608 / OM13092 ISP mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso54608 / OM13092 ISP mode

3,345 次查看
mirceaudrea
Contributor I

Hello,

I have a LPCXpresso54608 / OM13092 board and most probably I wrote the CRP incorrectly.

I get: Failed on connect: Ep(01). Target marked as not debuggable.

I need to erase the flash and regain debugger control. 

I tried to use Flash Magic with onboard LPC-LINK2(reset button +ISP0/1/2) on the serial port provided by it, but it cannot connect (cannot autobaud error).

Does the serial port on J13 connector provide ISP capabilities?

Is there another way in order to un-brick it?

Best regards,

Mircea

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

3,070 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Mircea Udrea,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.
Please refer to the attachment to assure the MCU enter the ISP mode successful via properly hardware configuration.
And I'd like to suggest another way to 'release' the LPC54608.
First, you should update the on-board LPC-Link2 with the JLink firmware,
then follow the Fig1 to work it out.
2017-04-27_10-27-44.jpgFig 1


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,070 次查看
mirceaudrea
Contributor I

Did the job!

Thanks.

0 项奖励
回复