LPCXpresso LPC1769 Emulator Not Found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso LPC1769 Emulator Not Found

3,102 Views
yi_wang
Contributor I

hi all,

I am new here and just begin to work with the LPCXpresso LPC1769 eva-board for one demo project.

I installed LPCXpresso V8.22_650 IDE, LPC11Uxx-Debug-Probe-VCOM driver in my Win7 X64 system.

With the example programs I am able to compile, build, but not with debug or download to processor.

The error log is

"No compatible emulators available.
They may be disconnected, not powered, already in use or not compatible with this target".

However my eva-board is conneted without problem. I've tried all "shown Debugger" setting like "LPC-Link (WinUSB) or RDB-Link // LPC-Link (HID) //  Red Probe Family // Link Server", but nothing changed.

So can someone help me to solve this issue? Thanks so much.

Regards,

Yi

Labels (3)
0 Kudos
Reply
3 Replies

2,979 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, WangYi,

Do you use the keil board?

pastedImage_1.png

If you use the board, what is the debug device you are using? which connector are you using?

BR

Xiangjun Rong

0 Kudos
Reply

2,979 Views
yi_wang
Contributor I

Hello Xiangjun,

thanks for your reply.

No, I don't have the Keil LPC1769 you showed.

I have in hand the OM13085 eva board.

65656565.JPG

In principle I don't need any further HW component more.

BR,

Yi

0 Kudos
Reply

2,978 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, WangYi,

I suggest you refer to the two figures, I use a board on which the  LPC11U35 CMSIS-DAP chip is embedded. On the device manager menu, the LPC11U35 is enumerated as LPC11U3x CMSIS-DAP device.

I use MCUXpresso IDE tools.

Hope it can help you

BR

Xiangjun Rong

pastedImage_3.png

pastedImage_2.png

0 Kudos
Reply