LPCXpresso LPC1347 Rev A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso LPC1347 Rev A

1,656件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sat Nov 15 08:59:44 MST 2014
Quite a while ago, I bought an EA 1347 board (I.e. a LPC-Link [1] plus target)

Blowing the dust off, I plugged in the LPC-Link USB end.
The LED on the target flashes twice every second, so I guessed that it comes pre-loaded with something.

After a bit of a struggle, I have captured the flash contents.

 000047C0  ····0123456789abcdef·····***************************************
 00004800  ******************···*···* (C) 2012 Embedded Artists AB··* Welco
 00004840  me to the LPCXpresso LPC1347 demo program v1.0···* - Flashing LE
 00004880  D····* This program is also a test agent for production tests.··
 000048C0  ·* It response to EA commands...····%c···%s··FAIL:Resetting inpu
 00004900  t data;··Found terminating character as %d···[%d] %c·····Reached
 00004940   buff max (%d)··USB HID already ON··USB HID already OFF·········
 00004980  ·············&··u·······················!·····)·····2··········!
 000049C0  ····"!······· ······ ·······&·N·X·P· ·S·e·m·i·c·o·n·d·u·c·t·o·r·
 00004A00  s···L·P·C·1·3·4·x· ·H·I·D· ···D·E·M·O· · · · · · · ·E·A···H·I·D·
 00004A40  ··Serial initialized······hwUSB_Init error!!!······· ····5······
 00004A80  ·\···j··@w········!···$·@·'··2)· @,·`M/···0·@·3··{·············@


This appears to be a demo by EA.

I could not find the source bundle for this nor (more importantly) the PC program
(and its source code I hope) that excercises the demo. On the EA site. It just refers
back to the IDE and this forum, but nowhere specific.

Can anyone provide links for the above. Or, indeed, shed any light on the matter.

Cheers, Mike
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,599件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sun Nov 16 02:21:31 MST 2014
Thank you muchly, I have IDE 5.0.10 through 5.2.6 archived; I will investigate those.
Mike.
0 件の賞賛
返信

1,599件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sat Nov 15 10:26:51 MST 2014

Quote: MikeSimmonds
Can anyone provide links for the above. Or, indeed, shed any light on the matter.



:quest:

It's a 2012 (V5) sample: http://www.lpcware.com/lpcxpresso/downloads/older
0 件の賞賛
返信