Now Available: LPCXpresso for MAC OS X

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Now Available: LPCXpresso for MAC OS X

1,082件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by  on Thu Jul 12 16:08:23 MST 2012
<h1 id="post_message_17662"><strong><strong>NXP announces LPCXpresso for MAC OS X</strong></strong></h1>

In response to the high volume of user requests, NXP and Code Red are proud to announce the immediate availability of LPCXpresso for Mac OS X. Combined with the existing Windows and Linux support, this makes LPCXpresso a true multi-platform development environment.

To download and for more information, visit: <a href="http://lpcxpresso.code-red-tech.com/LPCXpresso/" target="_blank"><span style="text-decoration: underline;">http://www.lpcware.com/content/project/nxp-lpcxpresso</span></a>

ラベル(1)
0 件の賞賛
返信
0 返答(返信)