LPCOpen support or porting instructions for LPC12xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCOpen support or porting instructions for LPC12xx

1,475 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Whasssaaahhh on Mon Jun 10 07:03:36 MST 2013

Hello,


I'm considering to use LPCOpen for my projects, however, it seems there's no support for the 12xx currently. Is there a porting guide somewhere for 'non supported' processors ?


Labels (1)
0 Kudos
Reply
1 Reply

1,373 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Wed Jul 17 11:12:29 MST 2013
I agree with you, so I posted to the LPCWare my concern.

A workaround is to copy an existing driver for a similar part number, and then to use it in your LPC1227 projects. Luckily almost all peripherals in any LPC1xxx are the same, so that task is not that difficult. However, when you do so, look at the user manual to check you can use it as is.
0 Kudos
Reply