LPCOpen support or porting instructions for LPC12xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCOpen support or porting instructions for LPC12xx

1,513件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Whasssaaahhh on Mon Jun 10 07:03:36 MST 2013

Hello,


I'm considering to use LPCOpen for my projects, however, it seems there's no support for the 12xx currently. Is there a porting guide somewhere for 'non supported' processors ?


ラベル(1)
0 件の賞賛
返信
1 返信

1,411件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Wed Jul 17 11:12:29 MST 2013
I agree with you, so I posted to the LPCWare my concern.

A workaround is to copy an existing driver for a similar part number, and then to use it in your LPC1227 projects. Luckily almost all peripherals in any LPC1xxx are the same, so that task is not that difficult. However, when you do so, look at the user manual to check you can use it as is.
0 件の賞賛
返信