LPCOpen master SPI on 5410x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCOpen master SPI on 5410x

7,348 Views
selportion
Contributor I

Hello,

I am trying to setup a simple master SPI interface on LPC54102 using LPCOpen. Following the examples, I use:

Chip_Clock_EnablePeriphClock(SYSCON_CLOCK_SPI0);
SPI_CFGSETUP_T spiSetup;
SPIM_DELAY_CONFIG_T masterDelay;
Chip_SPI_Init(LPC_SPIMASTERPORT);
Chip_SPI_Enable(LPC_SPIMASTERPORT);
spiSetup.master = 1;
spiSetup.lsbFirst = 0;
spiSetup.mode = SPI_CLOCK_MODE0;
Chip_SPI_ConfigureSPI(LPC_SPIMASTERPORT, &spiSetup);
Chip_SPI_SetCSPolLow(LPC_SPIMASTERPORT, 0);
Chip_SPIM_SetClockRate(LPC_SPIMASTERPORT, LPCMASTERCLOCKRATE);
masterDelay.PreDelay = 0x4;
masterDelay.PostDelay = 0x4;
masterDelay.FrameDelay = 0x4;
masterDelay.TransferDelay = 0x4;
Chip_SPIM_DelayConfig(LPC_SPIMASTERPORT, &masterDelay);
Chip_SPI_EnableInts(LPC_SPIMASTERPORT, (SPI_INTENSET_RXDYEN | SPI_INTENSET_SSDEN)); //???Needed?
NVIC_EnableIRQ(LPC_SPIMASTERIRQNUM);
spiMasterXfer.cbFunc = master_cb;
spiMasterXfer.state = SPIS_XFER_STATE_IDLE;
spiMasterXfer.txBuff = masterTXBuffer16;
spiMasterXfer.txCount = sizeof(masterTXBuffer16) / sizeof(uint16_t);/* Count is in transfer size */
spiMasterXfer.rxBuff = masterRXBuffer16;
spiMasterXfer.rxCount = sizeof(masterRXBuffer16) / sizeof(uint16_t);/* Count is in transfer size */
mstate = &spiMasterXfer.state;
spiMasterXfer.options = SPIM_XFER_OPTION_SIZE(16) | SPIM_XFER_OPTION_EOT | SPIM_XFER_OPTION_EOF;
spiMasterXfer.sselNum = 0;
masterTXBuffer16[0] = 0x1111;
Chip_GPIO_SetPinOutHigh(LPC_GPIO, 0, 19);
Chip_SPIM_XferBlocking(LPC_SPIMASTERPORT, &spiMasterXfer);
while (*mstate != SPIM_XFER_STATE_DONE) {
__NOP();
}
Chip_GPIO_SetPinOutLow(LPC_GPIO, 0, 19);
masterTXBuffer16[0] = 0x2222;
Chip_GPIO_SetPinOutHigh(LPC_GPIO, 0, 19);
Chip_SPIM_XferBlocking(LPC_SPIMASTERPORT, &spiMasterXfer);
while (*mstate != SPIM_XFER_STATE_DONE) {
__NOP();
}
Chip_GPIO_SetPinOutLow(LPC_GPIO, 0, 19);

To my surprise, I see the gpio toggling 4 times before even the first slave-select. The first word is sent (0x1111), then after a very long, unexplained delay also the second word comes (0x2222). There is no pulsing of the SlaveSelect signal in between, despite the
SPIM_XFER_OPTION_EOT | /* Enable this to assert and deassert SSEL for each individual byte/word */

Am I doing something inherently wrong?
Thank you for your support

Labels (2)
0 Kudos
Reply
4 Replies

6,762 Views
selportion
Contributor I

I still don't know if my configuration is wrong or if LPCOpen does not correctly support a simple blocking Master SPI read-write for this chip...

If anyone in the future runs into the same problem, the following works:

void spi_init(void) {

Chip_Clock_EnablePeriphClock(SYSCON_CLOCK_SPI0);
Chip_SYSCON_PeriphReset(RESET_SPI0);
LPC_SPIMASTERPORT->CFG = (SPI_CFG_MASTER_EN | SPI_CFG_SPI_EN);
LPC_SPIMASTERPORT->DLY = (SPI_DLY_PRE_DELAY(4) | SPI_DLY_POST_DELAY(4) | SPI_DLY_FRAME_DELAY(4) | SPI_DLY_TRANSFER_DELAY(4));
Chip_SPIM_SetClockRate(LPC_SPIMASTERPORT, LPCMASTERCLOCKRATE);
LPC_SPIMASTERPORT->TXCTRL = (SPI_TXCTL_EOT | SPI_TXCTL_EOF | SPI_TXCTL_FLEN(16));

}

uint16_t spi_send_receive(uint16_t txdata) {

while (!(LPC_SPIMASTERPORT->STAT & SPI_STAT_TXRDY)) { __NOP(); }
LPC_SPIMASTERPORT->TXDAT = (uint32_t)txdata;
while ((!(LPC_SPIMASTERPORT->STAT & SPI_STAT_TXRDY))||(!(LPC_SPIMASTERPORT->STAT & SPI_STAT_RXRDY))) { __NOP(); }
return (uint16_t)((LPC_SPIMASTERPORT->RXDAT)&0xff);

}

Without using interrupts or callbacks

0 Kudos
Reply

6,762 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Patroklos Anagonostou,

   Sorry for my later reply!

   I have test the lpcopen spi master in my LPCXpresso 54102 board, the GPIO PIO0_19 can track the SPI wave correctly.

   This is my logic analyzer SPI wave

pastedImage_1.png

Clock rate is 4Mhz.

pastedImage_2.png

My modified code is lpc5410x_xpresso54102_keil_iar_v3.03.000_16, project periph_spi_sm_int.

Main code is :

int main(void)
{
     int loop = 1;     /* Prevents unreachable statement warning */
     uint16_t seed = 0;
     volatile uint8_t *mstate, *sstate;

     SystemCoreClockUpdate();
     Board_Init();

                Chip_GPIO_SetPinDIROutput(LPC_GPIO, 0, 19);
          Chip_GPIO_SetPinState(LPC_GPIO, 0, 19, true);
                Chip_GPIO_SetPinOutHigh(LPC_GPIO, 0, 19);
     /* SPI initialization */
     Init_SPI_PinMux();

     /* Initialize stopwatch driver so some event times can be measured */
     StopWatch_Init();

     /* Setup SPI controllers */
     setupMaster();
     setupSlave();

     /* Enable SPI controller interrupts */
     NVIC_EnableIRQ(LPC_SPIMASTERIRQNUM);
     NVIC_EnableIRQ(LPC_SPISLAVEIRQNUM);

     DEBUGOUT("SPI master/slave combined example\r\n");

     /* Loop forever */
     while (loop) {
          /* Setup some data for transmit from master to slave and slave to master */
          seed = bufferInit(seed);
                masterTXBuffer16[0] = 0X1111;
                masterTXBuffer16[1] = 0X2222;

          /* Set master transfer, this is only the initial trasnfer, the callbacks can
             change this later */
          spiMasterXfer.cbFunc = master_cb;
          spiMasterXfer.state = SPIS_XFER_STATE_IDLE;
          spiMasterXfer.txBuff = masterTXBuffer16;
          spiMasterXfer.txCount = 1;/* Count is in transfer size */
          spiMasterXfer.rxBuff = masterRXBuffer16;
          spiMasterXfer.rxCount = 1;/* Count is in transfer size */
          mstate = &spiMasterXfer.state;

          /* Setup master trasnfer options - 16 data bits per transfer, EOT, EOF */
          spiMasterXfer.options =
               SPIM_XFER_OPTION_SIZE(16) |          /* This must be enabled as a minimum, use 16 data bits */
               SPIM_XFER_OPTION_EOT |               /* Enable this to assert and deassert SSEL for each individual byte/word, current slave functions for this example do not support this */
               SPIM_XFER_OPTION_EOF |               /* Insert a delay between bytes/words as defined by frame delay time */
               0;

          /* Use SPI select 0 */
          spiMasterXfer.sselNum = 0;

          /* Time master and slave transfers */
          masterTime = StopWatch_Start();

          /* Limitation: The call below 'pre-buffers' the initial slave transmit datum.
             If this isn't pre-buffered, a slave transmit underflow will always occur
               at slave assertion time for the initial transmit datum. The datum sent to the
               master will be 0. This is ok as we are only using a single slave, but with multiple
               slaves pre-buffering is not always an option and the master might need to toss the
               first byte. */
          Chip_SPI_FlushFifos(LPC_SPIMASTERPORT);
                Chip_GPIO_SetPinOutHigh(LPC_GPIO, 0, 19);
          /* Start master transfer */
          Chip_SPIM_Xfer(LPC_SPIMASTERPORT, &spiMasterXfer);
          /* Sleep until transfers are complete */
          while ((*mstate != SPIM_XFER_STATE_DONE) ) {
               //__WFI();
          }
              Chip_GPIO_SetPinOutLow(LPC_GPIO, 0, 19);
              
              //===============================
           spiMasterXfer.cbFunc = master_cb;
          spiMasterXfer.state = SPIS_XFER_STATE_IDLE;
          spiMasterXfer.txBuff = masterTXBuffer16+1;
          spiMasterXfer.txCount = 1;/* Count is in transfer size */
          spiMasterXfer.rxBuff = masterRXBuffer16;
          spiMasterXfer.rxCount = 1;/* Count is in transfer size */
          mstate = &spiMasterXfer.state;

          /* Setup master trasnfer options - 16 data bits per transfer, EOT, EOF */
          spiMasterXfer.options =
               SPIM_XFER_OPTION_SIZE(16) |          /* This must be enabled as a minimum, use 16 data bits */
               SPIM_XFER_OPTION_EOT |               /* Enable this to assert and deassert SSEL for each individual byte/word, current slave functions for this example do not support this */
               SPIM_XFER_OPTION_EOF |               /* Insert a delay between bytes/words as defined by frame delay time */
               0;

          /* Use SPI select 0 */
          spiMasterXfer.sselNum = 0;

          /* Time master and slave transfers */
          masterTime = StopWatch_Start();

          /* Limitation: The call below 'pre-buffers' the initial slave transmit datum.
             If this isn't pre-buffered, a slave transmit underflow will always occur
               at slave assertion time for the initial transmit datum. The datum sent to the
               master will be 0. This is ok as we are only using a single slave, but with multiple
               slaves pre-buffering is not always an option and the master might need to toss the
               first byte. */
          Chip_SPI_FlushFifos(LPC_SPIMASTERPORT);
                Chip_GPIO_SetPinOutHigh(LPC_GPIO, 0, 19);
          /* Start master transfer */
          Chip_SPIM_Xfer(LPC_SPIMASTERPORT, &spiMasterXfer);
          /* Sleep until transfers are complete */
          while ((*mstate != SPIM_XFER_STATE_DONE) ) {
               //__WFI();
          }
              Chip_GPIO_SetPinOutLow(LPC_GPIO, 0, 19);             
          /* Toggle LED */
          Board_LED_Toggle(0);


          while (Board_UARTGetChar() == EOF) {}
     }



     return 0;
}
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

I also attached my spi_sm_int.c file for your reference.

You can try my code on your side.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

6,762 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Patroklos Anagnostou,

   Could you please also attach your SPI wave? Just for analysis.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

6,756 Views
selportion
Contributor I

Yes, please find attached the case with spi clock 1Mhz and the case with 100kHz.

The blue trace is the gpio that tracks the code execution flow, the green is the slave select, the yellow is clock and the pink is data. It seems to me that the spi functions are not blocking and the state is 'DONE' even during the transfer. Also in the case of 1Mhz the EOF flag to pulse the SS between byte/words is ignored.

0 Kudos
Reply