LPCOpen IAR Example Projects

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCOpen IAR Example Projects

2,215 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gregd on Thu Feb 28 19:45:24 MST 2013
Is there a target date for getting the IAR example projects back in the LPCOpen Platform.  I was hoping they would be included in this new release, but they weren't.

Thanks,
Greg
标签 (1)
0 项奖励
回复
3 回复数

2,182 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Fri Mar 01 16:23:00 MST 2013
Good point - Attached is a patch that provides IAR support for most of the 18xx/43xx periph_* group examples.
Just unpack the file onto your current v1.01 lpcopen tree.

The projects should work, but watch for issues. Start IAR with the workspace project in the lpc18xx_43xx/iar_ewarm_projects directory.

The clostest procedure for this is the LPC1347 IAR project quickstart guide.
http://docs.lpcware.com/lpcopen/_l_p_c_o_p_e_n_13_x_x__b_u_i_l_d_p_r_o_c_s__i_a_r.html
0 项奖励
回复

2,182 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jonper on Fri Mar 01 13:56:36 MST 2013
In the meantime, providing just a single buildable LPC43xx EWARM project with internal flash and ram targets would at least give us IAR users a head start on preparing to transition from the aging LPC43xx CMSIS. Can that be done?

Regards, John
0 项奖励
回复

2,182 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Fri Mar 01 13:11:00 MST 2013
Sorry about that, we stuffed as much as possible in the v1.01 release without altering the release date, but the IAR projects weren't ready yet.
These projects (for all supported boards) are the priority for the next v1.02 release. The release date for v1.02 is 03/22, but it might release early if the IAR projects are completed and reviewed before that. -Fingers crossed.-

http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers/lpcopen-upcoming-re...
0 项奖励
回复