LPC8N04 match register size

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC8N04 match register size

跳至解决方案
2,044 次查看
ppaw
Contributor I

I recently started working with LPC8N04 and as I'm quite new to this, I just lost a ton of time with CTIMER match register size. Variable used in the driver code for it has size of 32 bits (uint32_t), which in theory is the same in the microcontroller documentation, but after reading into it, only first 16 bits are used and the rest is reserved. I didn't know that at the beginning and only after a long time I found out that it is not the fault of my code, but the value that I assigned gets later cut down to 16 bits.

So my question is why do they use uint32_t, with no warning about it (except for one place in the MCU documentation), if they could easily use uint16_t instead?

标签 (1)
0 项奖励
回复
1 解答
2,011 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi ppaw

I understand your questions. LPC8N04 has two CTIMERs 16bit timer(CT16B) and 32bit timer(CT32B).

Accordingly, MR is 16bit for CT18B and 32bit for CT32B.

both of CTIMERs use CTIMER_SetupMatch to setup match register.

I checked, its indeed no judgement in this function for CT16B. It will be good to add a warning  inside this function for CT16B if MR over 16bit.

I will suggest it to SDK development team. Thanks.

 

Best Regards

Jun Zhang

 

 

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,024 次查看
ppaw
Contributor I

Hi ZhangJennie,

I'm using SDK: SDK_2.x_LPC8N04DevBoard. I based my code on demo ctimer_match_example, but I'm not sure how can I find a direct link to it.

In the base version of the example, it works because the value assigned to the matchValue: "matchConfig.matchValue = EXAMPLE_CTIMER_CLK_FREQ / 10;" can fit into 16 bits. If you switch it eg: "matchConfig.matchValue = EXAMPLE_CTIMER_CLK_FREQ;" and in debug mode compare the value of matchConfig.matchValue and EXAMPLE_CTIMER.MR[0], you will see that:

matchConfig.matchValue = 500000 (binary 1111010000100100000)

EXAMPLE_CTIMER.MR[0] = 41248 (binary     1010000100100000) - cut down to 16 bits

Thanks,

ppaw

0 项奖励
回复
2,012 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi ppaw

I understand your questions. LPC8N04 has two CTIMERs 16bit timer(CT16B) and 32bit timer(CT32B).

Accordingly, MR is 16bit for CT18B and 32bit for CT32B.

both of CTIMERs use CTIMER_SetupMatch to setup match register.

I checked, its indeed no judgement in this function for CT16B. It will be good to add a warning  inside this function for CT16B if MR over 16bit.

I will suggest it to SDK development team. Thanks.

 

Best Regards

Jun Zhang

 

 

 

0 项奖励
回复
1,989 次查看
ppaw
Contributor I

Hi Jun Zhang,

Ok, I understand my mistake. Thanks a lot.

 

 

0 项奖励
回复
2,029 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI ppaw

Which demo code do you work with, any link?

if SDK, which version of it?

 

Thanks,

Jun Zhang

0 项奖励
回复