LPC845 serial number

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC845 serial number

3,775件の閲覧回数
p_barrega
Contributor I

Good morning,

I'm working with an LPC845 series and I discovered that, on the same microcontroller, if I read serial number with ISP interface I get a value but if I read the same by SWD interface I obtain an other value, only the signature is equal in both cases. Serial number is stored on a database and I read this value to generate a key for firmware update.

Why this behaviour?

Thank you.

Have a nice day.

Pasquale Barrega.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,702件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi Pascual,

Sorry for the delay,

I am assuming that you are  trying to reading the UID (which is 128 bit wide).

I would take as valid the UID  returned by the ISP/IAP commands.  However, I am not  fully aware of your procedure for reading the numbers using SWD.  

It may be possible that the SWD is pointing different to a different memory location. 

Could you provide a screenshot  or the serial numbers  you  are reading ?

Regards,

Diego.

0 件の賞賛
返信

3,698件の閲覧回数
p_barrega
Contributor I

Hi Diego,

attached to this e-mail you can view two screenshots that show the Unique ID number read by ISP command and by SWD tool, precisely LPC-Link2.

To read this value I used the software Flash magic with it’s gui.

Best Regards.

Pasquale Barrega

Da: diego.charles <[email protected]>

Inviato: mercoledì 17 giugno 2020 01:53

A: Barrega Pasquale <[email protected]>

Oggetto: Re: - Re: LPC845 serial number

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: LPC845 serial number

reply from Diego Charles<https://community.nxp.com/people/diego.charles?et=watches.email.thread> in LPC Microcontrollers - View the full discussion<https://community.nxp.com/message/1327613?commentID=1327613&et=watches.email.thread#comment-1327613>

0 件の賞賛
返信

3,698件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi Pascual,

Thank you for your reply,

 I suggest you  to check the iap_basic example on the SDK .  It will help us to determine which number is valid.

Please, let me know your results.

Best regards,

Diego.

0 件の賞賛
返信