LPC845 sampling time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC845 sampling time

2,277件の閲覧回数
pasqualebarrega
Contributor II

Good morning, I'm working with an LPC845 microcontroller.

For a specific application I need to know how many TAD implies the sampling process of the A/D converter over the entire conversion time.

I have searched on user manual and datasheet but I haven't found any data about sampling except for the total conversion time that is equal to 25 TAD.

Thank you in advance.

Best regards.

Pasquale Barrega.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,159件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pasquale Barrega,

     The LPC845 didn't provide the other sample time, you can consider the full conversion time as the sample time.

pastedImage_1.png

So, if your ADC clock is the maximum data 30Mhz, then you will get the max conversion rate or sample rate 1.2Msample/s.

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,159件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pasquale Barrega,

   Could you give me the full name of TAD?

 

Best Regards,

Kerry

0 件の賞賛
返信

2,159件の閲覧回数
pasqualebarrega
Contributor II

Il 2019-02-20 12:21 kerryzhou ha scritto:

NXP COMMUNITY

RE: LPC845 SAMPLING TIME

reply from Kerry Zhou in LPC Microcontrollers - View the full

discussion

0 件の賞賛
返信