LPC845 sampling time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC845 sampling time

2,270 次查看
pasqualebarrega
Contributor II

Good morning, I'm working with an LPC845 microcontroller.

For a specific application I need to know how many TAD implies the sampling process of the A/D converter over the entire conversion time.

I have searched on user manual and datasheet but I haven't found any data about sampling except for the total conversion time that is equal to 25 TAD.

Thank you in advance.

Best regards.

Pasquale Barrega.

标签 (1)
0 项奖励
回复
3 回复数

2,152 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pasquale Barrega,

     The LPC845 didn't provide the other sample time, you can consider the full conversion time as the sample time.

pastedImage_1.png

So, if your ADC clock is the maximum data 30Mhz, then you will get the max conversion rate or sample rate 1.2Msample/s.

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

2,152 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pasquale Barrega,

   Could you give me the full name of TAD?

 

Best Regards,

Kerry

0 项奖励
回复

2,152 次查看
pasqualebarrega
Contributor II

Il 2019-02-20 12:21 kerryzhou ha scritto:

NXP COMMUNITY

RE: LPC845 SAMPLING TIME

reply from Kerry Zhou in LPC Microcontrollers - View the full

discussion

0 项奖励
回复