LPC844M201JHI48 Part Identification Number?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC844M201JHI48 Part Identification Number?

5,108件の閲覧回数
starblue
Contributor III

In the user manual the ISP part identification number of LPC844M201JHI48 is specified as 0x00008442, the same as for LPC844M201JBD48.  From looking at the LPC845 codes I guess the correct number is 0x00008443, is that right?

The context is that I'm just updating lpc21isp for the new LPC84x parts.

Regards

Jürgen

タグ(2)
0 件の賞賛
返信
5 返答(返信)

4,724件の閲覧回数
starblue
Contributor III

Any news on what the correct part id for LPC844M201JHI48 is?

Regards

Jürgen

0 件の賞賛
返信

4,724件の閲覧回数
ckphua
NXP Employee
NXP Employee

The corrected table29

pastedImage_1.png

4,724件の閲覧回数
ckphua
NXP Employee
NXP Employee

The User Manual Table 29 still need to be corrected.

0 件の賞賛
返信

4,724件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Table 29 in user manual, shows the LPC84x device ID register values:

pastedImage_1.png

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,724件の閲覧回数
starblue
Contributor III

The problem is that this table shows identical part ids for two different devices, so it can't be correct.

Regards

Jürgen

0 件の賞賛
返信