LPC844 examples for Keil

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC844 examples for Keil

2,847件の閲覧回数
KoComputes
Contributor II

Hi all, I'ld appreciate some advice to become productive with the LPC844 in Keil MDK.

The project uses I2C, SPI, GPIO and the ADC. I would like to have a printf() available for debugging, too.

1. where can I find working examples for LPC844 for Keil? Are they available? I can't see them in the pack installer.

2. what library stack should I work with? My first and only priority is development speed. So it must be intuitive and well documented.

- CMSIS

- NXP libraries from examples

- FSL libraries from examples

- ??

I'm using Keil UVision MDK 5.33, Segger J-Link debug probe on Windows 10.

 

Thanks!

0 件の賞賛
返信
5 返答(返信)

2,821件の閲覧回数
KoComputes
Contributor II

Thank you. How can I install the SDK files ?

It is not a uVision software pack. I made sure that 'Keil' was selected.

0 件の賞賛
返信

2,809件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Under SDK there is Getting Started with MCUXpresso SDK.pdf

Have a look on this chapter: Run a demo using Keil® MDK/μVision

This will tell you how to run a Keil demo.

 

Have a nice day,

Jun Zhang

0 件の賞賛
返信

2,790件の閲覧回数
KoComputes
Contributor II

Thank you. I wasn't aware that guides for Keil are part of the MCUXpresso SDK documentation.

I got the examples working. Nice, very helpful.

Regarding the second part of my question: I will go with the fsl_ drivers, the CMSIS software pack, and study CMSIS and the SDK docs first.

0 件の賞賛
返信

2,785件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Good to know. You are welcome!

0 件の賞賛
返信

2,828件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

we have MCUXpresso SDK for Keil. 

Here is the download site: https://mcuxpresso.nxp.com/en/builder?hw=LPC844

ZhangJennie_0-1616051930942.pngZhangJennie_0-1616051930942.png

 

Have a nice day

Jun Zhang

 

0 件の賞賛
返信