LPC844 ISP entry pin timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC844 ISP entry pin timing

1,143件の閲覧回数
r_poelstra
Contributor II

Hi,

 

I've a rather large capacitor connected to the ISP entry pin due to EMC issues. I'm using an LPC844.

I now have the problem that the part sometimes enters ISP mode on boot due to the capacitor not charging fast enough.

Is there any timing information available for the ISP entry pin so I can make sure that either the capacitor gets charged fast enough or that the reset signal is delay just long enough?

Please note that I want to keep the ISP entry feature, as there is also a button connected to force ISP mode. So I can't just disable it in FAIM/CRP.

 

Thanks in advance.

 

Kind regards,

 

Remco Poelstra

ラベル(1)
0 件の賞賛
返信
0 返答(返信)