LPC844 DAC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,552件の閲覧回数
tyassin1
Contributor II

Hi,

Simple question. Does the LPC844 have a DAC?
The ordering information say it is only LPC845, but going through the datasheet or manual in the pin configuration, nothing is written about this. It seems that both have the feature.

thank you.

0 件の賞賛
返信
1 解決策
1,538件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You are right, as the following ordering inf in data sheet of LPC84x, only LPC845 has the DAC module, the LPC844 does not have the DAC module.

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1677807936517.png

 

元の投稿で解決策を見る

1 返信
1,539件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You are right, as the following ordering inf in data sheet of LPC84x, only LPC845 has the DAC module, the LPC844 does not have the DAC module.

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1677807936517.png