LPC844 DAC?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC844 DAC?

跳至解决方案
1,593 次查看
tyassin1
Contributor II

Hi,

Simple question. Does the LPC844 have a DAC?
The ordering information say it is only LPC845, but going through the datasheet or manual in the pin configuration, nothing is written about this. It seems that both have the feature.

thank you.

0 项奖励
回复
1 解答
1,579 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You are right, as the following ordering inf in data sheet of LPC84x, only LPC845 has the DAC module, the LPC844 does not have the DAC module.

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1677807936517.png

 

在原帖中查看解决方案

1 回复
1,579 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You are right, as the following ordering inf in data sheet of LPC84x, only LPC845 has the DAC module, the LPC844 does not have the DAC module.

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1677807936517.png