LPC824 recommended quartz oscillator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC824 recommended quartz oscillator

1,037 Views
topspin
Contributor II

Hi all,

I am looking for a quartz oscillator to be used with the LPC824. I have seen that the LPCXpresso824-MAX Board uses the ABLS2-12.000MHZ-D4Y-T but it is too bluky for my new board (about 10mm length). Is there anything else with smaller footprint that you can recommend? Is ABM3B-12.000MHZ-B2-T a good replacement?

Best regards

Tags (1)
0 Kudos
Reply
1 Reply

1,019 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I think it is okay to use any 12MHz crystal with proper load capacitor.

so the ABM3B-12.000MHZ-B2-T is okay, the load cap is 18pF, so the two capacitor value is:

CX1=CX2=18pF*2=36pF.

Considering the parasitic cap, you can use 33pF cap for the CX1 and CX2.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply