LPC824(LPCOpen-project) porting to LPC845

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC824(LPCOpen-project) porting to LPC845

1,961 Views
lukaswipf
Contributor I

Is it possible to porting an existing LPC824 (LPCOpen) prject to the LPC845? The proble is that LPCOpen is not longer supported and there is no LPCOpen version for the LPC845. But I need to change the MCU because of more flash-space and I mustnot change my layout (they have the same Footprint/Pinout)

0 Kudos
Reply
2 Replies

1,553 Views
carstengroen
Senior Contributor II
0 Kudos
Reply

1,553 Views
jeremyzhou
NXP Employee
NXP Employee

Hi lukaswipf,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
1) Is it possible to porting an existing LPC824 (LPCOpen) prject to the LPC845?
Yes, you can do it.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply