LPC824(LPCOpen-project) porting to LPC845

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC824(LPCOpen-project) porting to LPC845

1,925件の閲覧回数
lukaswipf
Contributor I

Is it possible to porting an existing LPC824 (LPCOpen) prject to the LPC845? The proble is that LPCOpen is not longer supported and there is no LPCOpen version for the LPC845. But I need to change the MCU because of more flash-space and I mustnot change my layout (they have the same Footprint/Pinout)

0 件の賞賛
返信
2 返答(返信)

1,517件の閲覧回数
carstengroen
Senior Contributor II
0 件の賞賛
返信

1,517件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi lukaswipf,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
1) Is it possible to porting an existing LPC824 (LPCOpen) prject to the LPC845?
Yes, you can do it.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信