LPC812 XSON16 package information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC812 XSON16 package information

2,475 Views
jackhsu
Contributor III

Dear,

Good day.
I'm write the email that get more information about package XSON16.
We are IC programmer manufacturer, and we will support LPC812 with XSON16 for customer in China.
We are finding the socket on it. and the socket manufacturer ask us that he has to know the normal and minimum about the height of IC.
The height is only show maximum is 0.5mm, or let me know the tolerance about height of IC. Thanks.

There is the package information.
https://www.nxp.com/docs/en/package-information/SOT1341-1.pdf

Labels (1)
0 Kudos
Reply
3 Replies

2,318 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Jack

This is 0.45 to 0.50 mm

Regards

Vicente

0 Kudos
Reply

2,317 Views
jackhsu
Contributor III

Hi Vicente,

Thanks for your reply.

Is the 0.45mm typical or minimum?

Thank you.

Regards,

Jack Hsu

0 Kudos
Reply

2,317 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

0.45 mm is the minimum.

Regards

Vicente Gomez

0 Kudos
Reply