LPC812 XSON16 package information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC812 XSON16 package information

2,507件の閲覧回数
jackhsu
Contributor III

Dear,

Good day.
I'm write the email that get more information about package XSON16.
We are IC programmer manufacturer, and we will support LPC812 with XSON16 for customer in China.
We are finding the socket on it. and the socket manufacturer ask us that he has to know the normal and minimum about the height of IC.
The height is only show maximum is 0.5mm, or let me know the tolerance about height of IC. Thanks.

There is the package information.
https://www.nxp.com/docs/en/package-information/SOT1341-1.pdf

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,350件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Jack

This is 0.45 to 0.50 mm

Regards

Vicente

0 件の賞賛
返信

2,349件の閲覧回数
jackhsu
Contributor III

Hi Vicente,

Thanks for your reply.

Is the 0.45mm typical or minimum?

Thank you.

Regards,

Jack Hsu

0 件の賞賛
返信

2,349件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

0.45 mm is the minimum.

Regards

Vicente Gomez

0 件の賞賛
返信