LPC812: Flash access cycles

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC812: Flash access cycles

1,492 Views
karthikvenkates
Contributor II

Hi,

There is an option in LPC812 to select the number of System clock cycles taken for accessing Flash memory. We can select 1 cycle or 2 cycles.

pastedImage_1.png

My question is, why we are given this option ? Is it just a simple feature that lets us work on two different speeds or is there any specific reason for this option ? Why not 3 cycles or 4 cycles ?

Labels (2)
0 Kudos
Reply
1 Reply

1,270 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Karthik venkatesh,

   I think our lpc812 code can answer your questions clearly:

typedef enum {
    FLASHTIM_20MHZ_CPU = 0,        /*!< Flash accesses use 1 CPU clocks. Use for up to 20 MHz CPU clock*/
    FLASHTIM_30MHZ_CPU = 1,     /*!< Flash accesses use 2 CPU clocks. Use for up to 30 MHz CPU clock*/
} FMC_FLASHTIM_T;

/**
 * @brief    Set FLASH memory access time in clocks
 * @param    clks    : Clock cycles for FLASH access
 * @return    Nothing
 * @note    For CPU speed up to 20MHz, use a value of 0. For up to 30MHz, use
 *            a value of 1
 */
STATIC INLINE void Chip_FMC_SetFLASHAccess(FMC_FLASHTIM_T clks)
{
    uint32_t tmp = LPC_FMC->FLASHCFG & (~((0x3)|FMC_FLASHCFG_RESERVED));

    /* Don't alter upper bits */
    LPC_FMC->FLASHCFG = tmp | clks;
}

You just need to know, when the cpu clock is below20Mhz, you can use FLASHTIM =0, when the clock is up 20Mhz, and below 30Mhz, you need to use the FLASHTIM=1.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply