#LPC804: "Write to RAM" command sequence

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

#LPC804: "Write to RAM" command sequence

跳至解决方案
2,184 次查看
lucazanuttini
Contributor II
Hello All,

According to the UM11065 on page 25 of 355, the command handler should answer OK after receiving the raw data of the "Write to RAM" command. However, based on my tests, it does not answer instead.

Can you please confirm it?

 

I can perform all the other UART commands successfully.

 

Thanks in advance!

标签 (1)
0 项奖励
回复
1 解答
2,164 次查看
lucazanuttini
Contributor II

Hi Alice,

Thank you very much for your help.

I wasn't aware about AN13815. It is correct then to not have the "OK<CR><LF>" acknowledge from the device after the data is sent.

 

Best Regards,

Luca Zanuttini

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,167 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @lucazanuttini 

It seems the same question with your private ticket, I have reply you on that case.

You can contact me if still have issue on that ticket.

 

BR

Alice

0 项奖励
回复
2,165 次查看
lucazanuttini
Contributor II

Hi Alice,

Thank you very much for your help.

I wasn't aware about AN13815. It is correct then to not have the "OK<CR><LF>" acknowledge from the device after the data is sent.

 

Best Regards,

Luca Zanuttini

0 项奖励
回复