#LPC804: "Write to RAM" command sequence

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

#LPC804: "Write to RAM" command sequence

ソリューションへジャンプ
2,150件の閲覧回数
lucazanuttini
Contributor II
Hello All,

According to the UM11065 on page 25 of 355, the command handler should answer OK after receiving the raw data of the "Write to RAM" command. However, based on my tests, it does not answer instead.

Can you please confirm it?

 

I can perform all the other UART commands successfully.

 

Thanks in advance!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,130件の閲覧回数
lucazanuttini
Contributor II

Hi Alice,

Thank you very much for your help.

I wasn't aware about AN13815. It is correct then to not have the "OK<CR><LF>" acknowledge from the device after the data is sent.

 

Best Regards,

Luca Zanuttini

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,133件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @lucazanuttini 

It seems the same question with your private ticket, I have reply you on that case.

You can contact me if still have issue on that ticket.

 

BR

Alice

0 件の賞賛
返信
2,131件の閲覧回数
lucazanuttini
Contributor II

Hi Alice,

Thank you very much for your help.

I wasn't aware about AN13815. It is correct then to not have the "OK<CR><LF>" acknowledge from the device after the data is sent.

 

Best Regards,

Luca Zanuttini

0 件の賞賛
返信