LPC804 -> I2C Timeout Function when configured as slave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC804 -> I2C Timeout Function when configured as slave

2,112 Views
thomasboehmer
Contributor I

Hi all,

i want to use the timeout function of i2c peripheral when it is configured as slave. How can I do that? When i write to the timeout register the value isn't set to the register. Is there any sample Code?

Thanks

0 Kudos
Reply
3 Replies

1,575 Views
alikarakaş
Contributor I

You can find in lpc 804 user manual.

chrome-extension://efaidnbmnnnibpcajpcglclefindmkaj/https://www.mouser.com/pdfdocs/NXP_LPC804_UM.pdf

0 Kudos
Reply

2,046 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Thomas,

Unfortunately there isn't any example code to use the timeout functionality but I will suggest to check the chapter:

  • 15.7.2 Time-out: This chapter explains the modes where the time out can be used.
  • 15.6.5 Time-out value register: In the description of the register says which others registers need to be activated.

Let me know if this helps you.

Best Regards,

Alexis Andalon

1,734 Views
manoj_123
Contributor II
Hii sir,
How can I go through 15.7.2 chapter in which manual or datasheet it mentioned can tell me
0 Kudos
Reply