LPC804 -> I2C Timeout Function when configured as slave

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC804 -> I2C Timeout Function when configured as slave

1,992件の閲覧回数
thomasboehmer
Contributor I

Hi all,

i want to use the timeout function of i2c peripheral when it is configured as slave. How can I do that? When i write to the timeout register the value isn't set to the register. Is there any sample Code?

Thanks

0 件の賞賛
返信
3 返答(返信)

1,455件の閲覧回数
alikarakaş
Contributor I

You can find in lpc 804 user manual.

chrome-extension://efaidnbmnnnibpcajpcglclefindmkaj/https://www.mouser.com/pdfdocs/NXP_LPC804_UM.pdf

0 件の賞賛
返信

1,926件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Thomas,

Unfortunately there isn't any example code to use the timeout functionality but I will suggest to check the chapter:

  • 15.7.2 Time-out: This chapter explains the modes where the time out can be used.
  • 15.6.5 Time-out value register: In the description of the register says which others registers need to be activated.

Let me know if this helps you.

Best Regards,

Alexis Andalon

1,614件の閲覧回数
manoj_123
Contributor II
Hii sir,
How can I go through 15.7.2 chapter in which manual or datasheet it mentioned can tell me
0 件の賞賛
返信