LPC804 Unable To Flash after initial Flashing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC804 Unable To Flash after initial Flashing

1,441 次查看
TAG
Contributor I

Hi there,

I am having issues with my LPC804 (LPC80X ), whenever I initially flash the chip. The chip is no longer able to be detected by the debugger and is unable to be flashed. I have tried on both my custom board and the Development Board Section of the MCU-Link Pro and both have had the same outcome. When programming both with sample files they both worked prior to me programming my custom firmware, hence I am certain it is a software setup issue. From looking at the data sheets and such I believe it might be in the inital bootloader startup that is the issue, as I have removed the system_init(); function and system_lpc804 file from the build with the reset handler branching straight to main. Other than this I am unable to see what could be causing this issue and need some assistance.

My reset handler looks like this:

 

 

/* Reset Handler */

    .thumb_func
    .align 2
    .weak    Reset_Handler
    .type    Reset_Handler, %function

Reset_Handler:
    ldr   r0,=__main
    bx    r0

    .pool
    .size Reset_Handler, . - Reset_Handler

 

 

标记 (1)
0 项奖励
回复
1 回复

1,410 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @TAG 

Recommend program a simple SDK demo with Development Board. For example LED.

If you still have question about it, please kindly let me know.

BR

Alice

0 项奖励
回复