LPC804 Build Failed when enable link-time optimization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC804 Build Failed when enable link-time optimization

2,339件の閲覧回数
wangjn-maxeye
Contributor I

The build log:

Building target: application.axf
Invoking: MCU Linker
arm-none-eabi-gcc -nostdlib -L"H:\gerrit\WLC_LPC804\v11\Maxeye\source" -Xlinker -Map="application.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -mcpu=cortex-m0 -mthumb -T "App_USI141_Debug.ld" -o "application.axf" ./src/WlcDeviceApp.o ./src/WlcDeviceApp_Mcu.o  ./WlcDeviceLibrary/wlc_device/wlc_appproc.o ./WlcDeviceLibrary/wlc_device/wlc_chgproc.o ./WlcDeviceLibrary/wlc_device/wlc_crn120.o ./WlcDeviceLibrary/wlc_device/wlc_crn120cfg.o ./WlcDeviceLibrary/wlc_device/wlc_device.o ./WlcDeviceLibrary/wlc_device/wlc_ndef.o ./WlcDeviceLibrary/wlc_device/wlc_optional.o ./WlcDeviceLibrary/wlc_device/wlc_utility.o ./WlcDeviceLibrary/wlc_charge_rx/PCA943x/pca9430-charger.o ./WlcDeviceLibrary/wlc_charge_rx/PCA943x/pca9431-vout.o ./WlcDeviceLibrary/wlc_charge_rx/PCA943x/pca943x-adc.o ./WlcDeviceLibrary/wlc_charge_rx/PCA943x/pca943x-otp.o ./WlcDeviceLibrary/wlc_charge_rx/PCA943x/pca943x-rect.o ./WlcDeviceLibrary/wlc_charge_rx/PCA943x/pca943x-rxir.o ./WlcDeviceLibrary/wlc_charge_rx/PCA943x/pca943x-vpwr.o ./WlcDeviceLibrary/wlc_charge_rx/PCA943x/pca943x.o ./WlcDeviceLibrary/wlc_charge_rx/wlc_chg_rx_adc_pca.o ./WlcDeviceLibrary/wlc_charge_rx/wlc_chg_rx_charger_pca.o ./WlcDeviceLibrary/wlc_charge_rx/wlc_chg_rx_pca.o ./WlcDeviceLibrary/wlc_charge_rx/wlc_chg_rx_rxir_pca.o ./WlcDeviceLibrary/wlc_charge_rx/wlc_chg_rx_vout_pca.o ./WlcDeviceLibrary/wlc_charge_rx/wlc_chg_rx_vpwr_pca.o ./WlcDeviceLibrary/wlc_charge_rx/wlc_chg_rx_vrect_pca.o ./WlcDeviceLibrary/wlc_charge_rx/wlc_chg_rx_vtune_pca.o ./WlcDeviceLibrary/CRN120_1.0.0/HAL_CRN120/CRN120_driver.o ./SDK_2.7.0_LPC804/devices/LPC804/mcuxpresso/startup_lpc804.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_acomp.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_adc.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_capt.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_clock.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_common.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_crc.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_ctimer.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_dac.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_gpio.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_i2c.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_iap.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_mrt.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_pint.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_plu.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_power.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_reset.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_spi.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_swm.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_syscon.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_usart.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_wkt.o ./SDK_2.7.0_LPC804/devices/LPC804/drivers/fsl_wwdt.o ./SDK_2.7.0_LPC804/devices/LPC804/system_LPC804.o ./OSAL/src/LPC804SDK/phOsal_GPIO_LPC804.o ./OSAL/src/LPC804SDK/phOsal_I2C_LPC804.o ./OSAL/src/LPC804SDK/phOsal_IRQ_LPC804.o ./OSAL/src/phOsal_DbgPrintf.o ./OSAL/src/phOsal_Mutex.o ./OSAL/src/phOsal_Timer.o ./Maxeye/source/app_debug.o  
C:\Users\MAXEYE\AppData\Local\Temp\cceiCvFj.s: Assembler messages:
C:\Users\MAXEYE\AppData\Local\Temp\cceiCvFj.s:7286: Error: invalid offset, value too big (0x000017E8)
lto-wrapper.exe: fatal error: arm-none-eabi-gcc returned 1 exit status
compilation terminated.
c:/nxp/mcuxpressoide_11.3.1_5262/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.3.0.202008311133/tools/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld.exe: error: lto-wrapper failed
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:53: application.axf] Error 1
"make -r -j6 all" terminated with exit code 2. Build might be incomplete.

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,324件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Wang,

I do not suggest you check the "Link-time Optimization". This is the description for the " Link-time Optimization option" in MCUXpresso tools help.

 

7.5 Support for testing link-time optimizations

Tests for link-time optimizations usually require multiple source files that are compiled separately, perhaps with different sets of options. There are several special-purpose test directives used for these tests.

{ dg-lto-do do-what-keyword }

do-what-keyword specifies how the test is compiled and whether it is executed. It is one of:

assemble

Compile with -c to produce a relocatable object file.

link

Compile, assemble, and link to produce an executable file.

run

Produce and run an executable file, which is expected to return an exit code of 0.

The default is assemble. That can be overridden for a set of tests by redefining dg-do-what-default within the .exp file for those tests.

Unlike dg-do, dg-lto-do does not support an optional ‘target’ or ‘xfail’ list. Use dg-skip-if, dg-xfail-if, or dg-xfail-run-if.

{ dg-lto-options { { options } [{ options }] } [{ target selector }]}

This directive provides a list of one or more sets of compiler options to override LTO_OPTIONS. Each test will be compiled and run with each of these sets of options.

{ dg-extra-ld-options options [{ target selector }]}

This directive adds options to the linker options used.

{ dg-suppress-ld-options options [{ target selector }]}

This directive removes options from the set of linker options used.

xiangjun_rong_0-1641367647127.png

 

BR

XiangJun Rong

0 件の賞賛
返信

2,321件の閲覧回数
wangjn-maxeye
Contributor I

understood, thank you

0 件の賞賛
返信