LPC802 initial configuration for reset pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC802 initial configuration for reset pin

ソリューションへジャンプ
1,722件の閲覧回数
asier
Contributor III

Hi,

Is there anyway to get reset function disabled from pin PIO0_5 when power up MCU ? 

We've observed that this pin starts always with RESET function in it and then we must to disconnect this function from user's code. Is possible to initialize RESET disabled by default in PIO0_5 ? 

Thanks,

Asier.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,614件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Asier,

After power on, the PIO0_5/Reset pin functions as Reset in default, there is no way to disable the pin Reset function after power-on. After power-on, if you want to use the pin as PIO0_5, you have to use firmware to set the RESETN bit in PINASSIGN7.

Hope it can help.

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,615件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Asier,

After power on, the PIO0_5/Reset pin functions as Reset in default, there is no way to disable the pin Reset function after power-on. After power-on, if you want to use the pin as PIO0_5, you have to use firmware to set the RESETN bit in PINASSIGN7.

Hope it can help.

BR

XiangJun Rong

0 件の賞賛
返信