LPC802 external reset pin not pull-up when restating

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC802 external reset pin not pull-up when restating

2,352 次查看
join_ren
Contributor III

We are in the debugging LPC802.  
There is a probability that the reset pin will not pull up when restarting.


Please tell me how to solve it. Thanks.

Reset Pin SCH: 

reset SCH.JPG

LPC802 SCH

LPC802 SCH.JPG

Power & Reset 

Power Reset.JPG

标签 (1)
0 项奖励
回复
3 回复数

2,230 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
After having a brief review of the schematic, I don't find anything wrong with it, so I'd like to know what the ratio of boards encounters this phenomenon, I suspect that the phenomenon may be related to PCB manufacturing or soldering technique.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

2,230 次查看
join_ren
Contributor III

Hi Jeremyzhou:

Thanks for your support.

"There is a probability that the reset pin will not pull up when restarting."   

Actual testing : 

1、This is abnormal LPC802's PCB can be restarting on the computer.     Use 3.3v start-up time 2ms.

2、This is abnormal LPC802's PCB cann't be restarting on the customer device.   Use 3.3v start-up time 8ms.

Could you tell me special requirement for LPC802 start-up ? 

On the computer start up:

On PC.jpg

 

On the customer device start up:

On device.jpg

0 项奖励
回复

2,230 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thanks for your reply.
Regarding the phenomenon, you should check the hardware design, especially the power supply, external crystal, reset pin, they're essential components of the minimum system.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复