LPC802 DMA example code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC802 DMA example code

1,381件の閲覧回数
parker_yu
Contributor I

I check the latest SDK, there isn't DMA example code, any guide or example code can help us to use DAM on LPC802, thanks.

SDK_2.5.0_LPCXpresso802

LPC802_example_code_bundle_Keil_v1.1

ラベル(1)
0 件の賞賛
返信
1 返信

1,280件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

LPC824 has DMA engine sit on AHB bus. While, LPC802 doesn't have DMA engine there. see LPC802 use manual UM11045, 1.5 block diagram.

So there is no DMA demo code included in MCUXpresso SDK package.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------