LPC800 ISP commands conflict with LPC1800 ISP commands

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC800 ISP commands conflict with LPC1800 ISP commands

651 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Wed Jul 31 05:24:42 MST 2013
Dear NXP developers,

you must be joking, when using the same command code 'S' for 'read CRC check[u]s[/u]um on' LPC800 and for '[u]s[/u]et active boot flash bank' on LPC1800 |(
There aren't any charaters left, are there?

They do differ in parameter count at least, but I would not count on the LPC1800 ISP handler to reject S 0 1024\r\n for example...

Why not use 'X' for set eXecutable bank on LPC1800 or 'H' for Hash sum on LPC800. Or maybe use lowercase 's' for the less dangerous command
'checksum' LPC800 and for
标签 (1)
0 项奖励
回复
0 回复数