LPC800 ISP commands conflict with LPC1800 ISP commands

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC800 ISP commands conflict with LPC1800 ISP commands

639 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Wed Jul 31 05:24:42 MST 2013
Dear NXP developers,

you must be joking, when using the same command code 'S' for 'read CRC check[u]s[/u]um on' LPC800 and for '[u]s[/u]et active boot flash bank' on LPC1800 |(
There aren't any charaters left, are there?

They do differ in parameter count at least, but I would not count on the LPC1800 ISP handler to reject S 0 1024\r\n for example...

Why not use 'X' for set eXecutable bank on LPC1800 or 'H' for Hash sum on LPC800. Or maybe use lowercase 's' for the less dangerous command
'checksum' LPC800 and for
Labels (1)
0 Kudos
Reply
0 Replies