LPC55xx Secondary Bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55xx Secondary Bootloader

Jump to solution
3,629 Views
jonathanmccarro
Contributor II

HI,

There is an application note AN12327 (Firmware Update Using Secondary Bootloader) for the LPC55xx. I cant find the lpc55xx_dsdl demo code from within this application note. It doesn't exist inside the SDK when built with the SDK Builder. Can someone send me the project code or a link.

Thanks

Labels (1)
1 Solution
3,193 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jonathan Mc Carron,

You can download it from below:

https://www.nxp.com/docs/en/application-note-software/AN12327SW.zip 

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

2 Replies
3,193 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jonathan Mc Carron,

You can download it from below:

https://www.nxp.com/docs/en/application-note-software/AN12327SW.zip 

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,193 Views
jonathanmccarro
Contributor II

Thanks Alice for quick response and resolution!

0 Kudos
Reply