LPC55xx ADC: 16 bit ADC has (only) ENOB = 12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55xx ADC: 16 bit ADC has (only) ENOB = 12

1,408件の閲覧回数
danielholala
Senior Contributor II

Hi there,

the ADC for LPC55xx (e.g., LPC5528) has an ENOB of only 12.

That number seems quite low (e.g., compared to a 20 year old ADuC841 with 12-bit ADC that has an ENOB of 11.6).

I wonder why this is. Is it due to the fact that the LPC55's ADC has a lot of "missing codes"?

Thanks.
Daniel

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,386件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

The ENOB typical values you can see in "Table 40. 16-bit ADC static characteristics" of datasheet.

Hope it helps you.

Have a nice day!

0 件の賞賛
返信

1,380件の閲覧回数
danielholala
Senior Contributor II

Dear @_Leo_ ,

for, e.g., LPC5528, datasheet states an ENOB of 12.

I think that is quite a low value for a 16 bit ADC. Why is this? Is it due to the fact that the LPC55's ADC exhibits a "missing codes"  issue?

What is the effective resolution for DC signals (from, e.g., thermistor, strain gauge, potentiometer)?

Thanks.
Dan

0 件の賞賛
返信