LPC55S6x VREFP and VDDA connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S6x VREFP and VDDA connection

1,825 次查看
RBhagat
Contributor I

Hello,

We are using LPC55S6x for our design. We are using analog input signals which are dropped down to 2.5V max. We have connected VREFP to 2.5V and we wanted to understand voltage level allowable for VDDA pin.V

As per datasheet, it is mentioned VDDA range from 1.8V to 3.6V and VREFP range from 0.985V to VDDA

RBhagat_0-1643704821297.pngRBhagat_0-1643704821297.png

 

However as per AN13033, VDDA is range of 3.0V to 3.6V and VREFP is same as datasheet. Refer snapshot

RBhagat_1-1643704898297.pngRBhagat_1-1643704898297.png

 

We have following queries, can we connect VREFP and VDDA to same voltage level as 2.5V or do we have to connect VDDA to 3.3V and VREFP to 2.5V (as per required)

Kindly do revert on same at the earliest.

Thanks,

RB

标签 (1)
0 项奖励
回复
1 回复

1,802 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi RBhagat 

Please refer our latest datasheet which is correct

https://www.nxp.com.cn/docs/en/nxp/data-sheets/LPC55S6x_DS.pdf

VDDA Analog supply voltage for ADC is 1.8 - 3.6 V

Vrefp ADC positive reference voltage is 0.985 - VDDA V

 

Hope this helps,

Jun Zhang

0 项奖励
回复