LPC55S6x USB1 as full speed device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S6x USB1 as full speed device

1,678件の閲覧回数
jh0
Contributor IV

Hi,

I see in this topic...

https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-spee...

that USB1 can't be forced to device in full speed mode, but there is in user manual (UM11126), Table 834. USB1 device command/status register (DEVCMDSTAT) bit 21 (R/W):

Forced FS

0: Default - drive K chirp during reset, go through HS negotiation.

1: Force the device to FS, do not drive K chirp during reset.

If USB1 device can be forced to full speed, in this case USB1 controller supporting crystal-less operation like USB0 or not? With both USB0 and USB1 active as full speed device.

Regards,

JH

0 件の賞賛
返信
1 返信

1,620件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi jh0 

Yes, you are right. USB1 can be used as Full speed. Forced FS value was updated in REV 2.4, 2021,OCT 07

ZhangJennie_0-1688633122900.png

 

The thread you referred was posted in 2020. Please don't use it. 

Thanks,

Jennie

0 件の賞賛
返信