LPC55S69 multicore project fails to run Core 1 after hitting 'RESET' but debugs properly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 multicore project fails to run Core 1 after hitting 'RESET' but debugs properly

1,300件の閲覧回数
RyanM314
Contributor I

Hello NXP community,

I have been experiencing issues with getting my multicore project to work after flashing code, pressing 'Terminate All Debug Sessions', and then pressing the 'RESET' button on the LPC55S69-EVK. Likewise, I cannot get the code to run after I power cycle and reset the micro. If I just run the MCUXpresso debugger and click 'Terminate All Debug Sessions', my code works properly.

My debugger does not have any software breakpoints for timing issues but it automatically opens my core 1's main() function when the MCMGR_StartCore(...) function is run. After that, the Core 1 code works.

When pressing reset, my Core 0 code works up until that function call to MCMGR_StartCore(...) and then this function never returns since my status LED never activates. It seems there is an initialization issue on the Core 1 side. 

Does anyone have an idea why this might happen and how to resolve this issue?

ラベル(1)
0 件の賞賛
返信
1 返信

1,263件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello RyanM314,

Dose your project includes Semihost like printf ?

 

BR

Alice

0 件の賞賛
返信