LPC55S69 : minimal PRINCE write chunk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : minimal PRINCE write chunk

1,210件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hello !

I can see SDK example about encryption/description on fly to flash memory by using PRINCE engine.

/* Loading data into the PRINCE - controlled flash area.
Note, that following conditions must be met (otherwise the error is returned):
- whole PRINCE subregions (8k block) must be erased at once
- whole PRINCE subregions (8k block) must be loaded at once (no partial write allowed)

Do I understand right and 8KB is minimum size for write and erase ?

So it is not possible to erase 8KB at once and after that write 512 bytes sectors ?

Regards,

Eugene

ラベル(1)
0 件の賞賛
返信
1 返信

1,154件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Yes, your assumptions are correct.

Regards

Soledad

Have a nice day!

0 件の賞賛
返信