LPC55S69: crystal-less design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69: crystal-less design

ソリューションへジャンプ
2,368件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hello !

Do I understand right and MCU can be totally crystalless  ? And supports whole declared temperature range ?

PLL0 can use FRO_12MHz and generate 100 or 150 Mhz clocks without any problems.

SPi and I2C can use FRO_12Mhz for clocking ( SPI speed can be 10Mhz ?).

RTC can own FRO32KHz oscillator but it may be not so precise for keep calendar time.

Is this so ? How to calculate possible drift while 1 week ?

What can be problems if no any crystals is not in use ?

Regards,

Eugene

1 解決策
2,280件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Eugene,

 

LPC55S69 can be used without external crystal. However, you will not be able to use USB High-Speed without it and RTC will not be as accurate as using external crystal.

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,281件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Eugene,

 

LPC55S69 can be used without external crystal. However, you will not be able to use USB High-Speed without it and RTC will not be as accurate as using external crystal.

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------