LPC55S69 : adc reference voltages

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : adc reference voltages

2,368件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi !

In source code I can see the next enumeration :

/*!
* @brief Define enumeration of reference voltage source.
*
* For detail information, need to check the SoC's specification.
*/
typedef enum _lpadc_reference_voltage_mode
{
kLPADC_ReferenceVoltageAlt1 = 0U, /*!< Option 1 setting. */
kLPADC_ReferenceVoltageAlt2 = 1U, /*!< Option 2 setting. */
kLPADC_ReferenceVoltageAlt3 = 2U, /*!< Option 3 setting. */
} lpadc_reference_voltage_source_t;

But it is no any exact information in UM or DS about it.

Could you explain a bit  what option correspond to what settings ?

Regards,

Eugene

ラベル(1)
3 返答(返信)

2,259件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Eugene Hiihtaja,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The enum value is used to select the voltage reference as below shows.

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,259件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi jeremyzhou‌ !

Could you confirm if VREFP is implemented on scheme of LPC55S69-EVK in correct way.

I can see it connected to VDDA_TARGET. Or in this way it is good enough  reference voltage for ADC ?

br,Eugene

0 件の賞賛
返信

2,259件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Eugene Hiihtaja,

1) In this way it is good enough  reference voltage for ADC ?

-- Yes, it's Ok.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------