LPC55S69 : RTOS selection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : RTOS selection

6,598件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi !

I'm looking for lightweight OS what can utilize AHB privilege checks on secure and non-secure sides.

Looks like this feature require special code isolation due fact that privilege master can't execute non-privileged code.

Could you suggest what kind of OS can be used for full utilization of all Trustzone-M features of LPC55S69.

 

Regards,

Eugene

 

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

6,534件の閲覧回数
converse
Senior Contributor V

Take a look at SecureThingz.com (part of IAR). I don’t know their products, but I know they support LPC55S6x

6,531件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi !

Not so much information on the site about it.

With freeRTOS and other operation system like this it is possible to utilize almost all TZ-M features but not those 2 ( AHB privilege check.)

In this case privileged master can't execute non privileged code. It means special code reorganization required. Simple example, you need separate memset/memcpy for privileged and nonprivileged code.

 

Regards,

Eugene

 

0 件の賞賛
返信

6,466件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Eugene,

One alternative that fully supports Trustzone is the Azure RTOS ThreadX. You can find more information on its repository:

https://github.com/azure-rtos/threadx/tree/master/ports/cortex_m33

This OS is supported by Microsoft, so we do not have documentation on it but there are some resources on its official website:

https://azure.microsoft.com/en-us/services/rtos/

I hope that this helps!

Regards,
Gustavo

0 件の賞賛
返信

6,541件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Eugene,

You should be able to utilize the AHB privilege checks regardless of the OS you would be using. You should even be able to use this feature on a bareboard application. However, we do not have examples with this implementation so you would need to setup these privilege checks based on ARM’s Trustzone documentation.

My apologies for the inconvenience.

Regards,
Gustavo

0 件の賞賛
返信

6,530件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi !

With freeRTOS and other similar operation system like this it is possible to utilize almost all TZ-M features but not those 2 ( AHB privilege check.)

In this case privileged master can't execute non privileged code. It means special code reorganization required. Simple example, you need separate memset/memcpy for privileged and nonprivileged code.

 

Regards,

Eugene

 

0 件の賞賛
返信

6,570件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Eugene,

You may use either FreeRTOS or baremetal applications and take advantage of the Trustzone features. There are a couple of examples on the MCUXpresso SDK that should serve as a starting point.

The examples are under rtos examples and are called freertos_blinky_ns (and s) and freertos_mpu_ns (and s). And the rest of the examples without FreeRTOS are under trustzone examples.

I hope that this information helps!

Regards,
Gustavo

0 件の賞賛
返信

6,487件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi @gusarambula  !

I just wondering if I not well understood AHB privilege check feature of TZ-M of LPC55Sxx.

What kind of rules are forced in use in case of code, data and access to peripherals ?

I assume both MPUs are active as well.

 

Regards !

Eugene

 

0 件の賞賛
返信

6,558件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hello !

All of those examples are not utilize this feature. it require special code reorganization and may be even other RTOS.

At it would be nice to have some examples and applications for understand what actions need for 

handle this feature of TZ.

 

Regards,

Eugene

 

0 件の賞賛
返信